Solution


Garbage Truck On-Board Weighing

A garbage disposal company wants a system to weigh the load capacity of their garbage truck bins.


GarbageonboardWeighing Color

Summary

  • Customer Need / Challenge

    A garbage disposal company wants to test the load capacity of their garbage truck bins. They need a force measurement system that will show them when it has reached maximum capacity.

  • Interface Solution

    Interface’s solution is to customize four SSB Sealed Beam Load Cells under the garbage box body with customer required capacity installed on either side by the customer with truck manufacturers guidance. This insures they are following the transportation department’s safety requirement and the manufacturer’s. When trash continues to be piled inside the box body, it will push more force down onto the SSB Sealed Beam Load Cells. When maximum load capacity has been reached, the results can be reviewed and displayed when connected to the 4850 Battery Powered Bluetooth Weight Indicator in real time.

  • Results

    The customer was able to test the maximum load capacity of the garbage bin attached to the truck, so they know when to empty the truck’s garbage at the transfer station.

Materials


  • Four SSB Sealed Beam Load Cells
  • JB104SS 4-Channel Stainless Steel Junction Box
  • 4850 Battery Powered Bluetooth Weight Indicator

How it Works


  1. The SSB Sealed Beam Load Cells are installed by the customer with their truck manufacturer’s guidance to under the truck’s garbage box body, on opposite sides. This insures they are following the transportation department’s safety requirements and their manufacturer’s requirements.
  2. As more trash is collected into the box body, more force weight is added and measured using the SSB Sealed Beam Load Cells.
  3. All load beams are connected to the JB104SS 4-Channel Stainless Steel Junction Box, which is then connected to the 4850 Battery Powered Bluetooth Weight Indicator for the customer to review results in real time.

Download PDF